2024-01-12 05:02 AM
Hello,
I am trying to explore the STWIN Starter Kit (SensorTile Wireless Industrial Mode) functionality. My OS is Windows 11. I plan to collect data and train models, so I am trying to use Unicleo GUI to define the sensors to be used, the full scale, the sampling frequency or ODR (Output Data Rate). However, Unicleo does not detect the board ("port not open").
What I have done so far :
Also, I get the following error in "User messages tab" : "Port: COM3 Open Failed".
So, do I miss anything here?
Note: the same issue was posted by @Rita Ch. Unicleo canot connect to SensorTile.box. - STMicroelectronics Community , but it is not solved.
Thank you,
Anthony
Solved! Go to Solution.
2024-01-12 05:37 AM
I have just read that Unicleo-GUI doesn't support the STEVAL-STWINKT1B toolkit so I guess that explains the problem...
2024-01-12 05:37 AM
I have just read that Unicleo-GUI doesn't support the STEVAL-STWINKT1B toolkit so I guess that explains the problem...