cancel
Showing results for 
Search instead for 
Did you mean: 

STWINBX1 datalogger - crashes when using device_config.json on SD card

johngj
Senior

Why does the datalogger crash when I put a device_config.json file on the SD card ?

I created the device_config.json file using the Python GUI tool, saved it to the computer and then copied it to the root folder of the SD card. 

The only changes I made was to the accelerometers where I changed the range to 4g (with the exception of IIS2ICLX which was left at 3g).

I put the SD card in the STWINBX1 and pressed the RESET button.

When I try to start the log (by pressing the USER button) the software seems to crash.

The green LED (LED_1) stays in the state when the USER button was pressed (i.e. permanently on or off).

The board has to be reset, but then the same happens again if I try to start a log.

When I try to access the log files on the SD card on the computer, I get an error saying the directory is corrupt, so this probably shows that the software is crashing...

johngj_0-1720188455528.png

I cannot delete the folders, so I have to reformat the SD card.

I have attached a copy of the device_config.json file (note I had to rename the extension to .txt in order to attach).

 

2 REPLIES 2
SimonePradolini
ST Employee

Hello @johngj 

I'll replicate your setup to find the issue. For sure, I'll integrate the bugfix in the upcoming FP-SNS-DATALOG2 v2.2.0.

In the meantime, which sd card are you using? FP-SNS-DATALOG2 User Manual includes a list of tested and suggested sd card part number and a troubleshooting paragraph.

 

Best regards

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

The SD card is a 2GB Transcend card, part number TS2GUSD...

https://uk.rs-online.com/web/p/sd-cards/1871643 

https://docs.rs-online.com/3ea7/0900766b816fae97.pdf