2021-08-19 12:25 PM
Here are the software versions I'm using:
I run into this problem since I have added the X-CUBE-AI software pack. every time I open the X-CUBE-AI configuration window, I get the following error:
Clock and Peripheral parameters not set for best performance, automatically fix?
further inspection shows that the following configurations are modified every time I open the X-CUBE-AI configuration window:
This is extremely inconvenient and make experimenting with neural network very frustrating and impractical. Please fix / provide a workaround
2021-11-05 6:35 AM
I can confirm that this is happening for me as well.
My configuration:
Seeing as how this was originally posted in August and it is now November, is there any word from ST on this? I will second that this is very inconvenient for the project(s) on which I am about to start.
2023-04-22 11:45 PM
I also have this problem. May some person deal with it to help me ?