2024-03-20 08:49 AM
Hello everyone,
I am currently working on a DIY toy project and I need some advice on selecting the appropriate components. My project involves setting up real-time image recognition artificial intelligence, a compatible camera, and controlling servo motors to aim a cannon based on the position of a detected target.
After conducting some research, I have decided to use an STM32 board to host the AI and control the servo motors. However, I am a bit overwhelmed by the various options of STM32 boards available in the market, and I am not sure which one to choose for my specific project.
Additionally, I am also looking for a camera that is compatible with the chosen STM32 board, capable of providing high-quality images for real-time image recognition.
I would therefore like to seek your expertise in guiding me through the selection of the appropriate STM32 board and camera for my needs. If you have any recommendations or advice on specific models to use for this project, I would be extremely grateful.
To summarize, here is what I am looking for:
Thank you in advance for your invaluable assistance.
Best regards,
Solved! Go to Solution.
2024-03-20 09:55 AM - edited 2024-03-20 09:56 AM
Hello,
Check this Camera module based on the OV5640 image sensor offering a 5-Mpixel resolution with 8-bit color
See also these threads:
https://community.st.com/t5/stm32-mcus-embedded-software/camera-module-for-stm32/m-p/626393
2024-03-20 09:06 AM
Hello,
Have a look at this video on Youtube.
Hope it can give you a visibility for what you're looking for
2024-03-20 09:19 AM
For servo motor control, I think you need a timer (PWM output) available almost on all STM32 MCUs. You need just to check the availability of this output on the board.
2024-03-20 09:24 AM
What factors should I consider to check the compatibility of the multiple cameras I have with the card?
2024-03-20 09:35 AM
What factors should I consider to check the compatibility of the multiple cameras I have with the card?
Not sure I understood the question. The STM32 has only one camera interface instance called DCMI.
For more information about this interface you can refer to this AN5020 "Introduction to digital camera interface (DCMI) for STM32 MCUs"
2024-03-20 09:48 AM
What cameras at a reasonable price would you recommend if I decide to make my prototype with a Nucleo card?
2024-03-20 09:55 AM - edited 2024-03-20 09:56 AM
Hello,
Check this Camera module based on the OV5640 image sensor offering a 5-Mpixel resolution with 8-bit color
See also these threads:
https://community.st.com/t5/stm32-mcus-embedded-software/camera-module-for-stm32/m-p/626393
2024-03-20 10:00 AM - edited 2024-03-20 10:01 AM
As stated in the thread https://community.st.com/t5/stm32-mcus-embedded-software/what-camera-module-should-i-use-with-stm32f746g-discovery-board/td-p/84585
this Camera module is pin to pin compatible with the STM32F4DIS-CAM already used in the Youtube I've already shared.