2023-10-20 9:03 PM - edited 2023-10-20 9:11 PM
This is the model i use(through X cube ai 8.1.0)
By annalyze it ,the output should be float as below
But the auto generated code declare it as ai_i8,why?
and I can`t get result in the following way,I don`t konw the reason
Because of the limits ,I can only provide three files here.
I`d appreciate it if someone could answer my questions!!!
Solved! Go to Solution.
2023-11-10 6:40 AM
Hello @123456dad ,
this is due to the quantization of the model as explained in the UM2526 section 1.3:
so to improve CPU and hardware accelerator latency this conversion from float to the ai_i8 is needed.
Hope this answers your request .
BR
2023-11-10 6:40 AM
Hello @123456dad ,
this is due to the quantization of the model as explained in the UM2526 section 1.3:
so to improve CPU and hardware accelerator latency this conversion from float to the ai_i8 is needed.
Hope this answers your request .
BR