/** ****************************************************************************** * @file app_x-cube-ai.c * @author X-CUBE-AI C code generator * @brief AI program body ****************************************************************************** * @attention * * Copyright (c) 2023 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* * Description * v1.0 - Minimum template to show how to use the Embedded Client API * model. Only one input and one output is supported. All * memory resources are allocated statically (AI_NETWORK_XX, defines * are used). * Re-target of the printf function is out-of-scope. * v2.0 - add multiple IO and/or multiple heap support * * For more information, see the embeded documentation: * * [1] %X_CUBE_AI_DIR%/Documentation/index.html * * X_CUBE_AI_DIR indicates the location where the X-CUBE-AI pack is installed * typical : C:\Users\\STM32Cube\Repository\STMicroelectronics\X-CUBE-AI\7.1.0 */ #ifdef __cplusplus extern "C" { #endif /* Includes ------------------------------------------------------------------*/ #if defined ( __ICCARM__ ) #elif defined ( __CC_ARM ) || ( __GNUC__ ) #endif /* System headers */ #include #include #include #include #include #include "app_x-cube-ai.h" #include "main.h" #include "ai_datatypes_defines.h" #include "network.h" #include "network_data.h" /* USER CODE BEGIN includes */ #include "images.h" /* USER CODE END includes */ /* IO buffers ----------------------------------------------------------------*/ #if !defined(AI_NETWORK_INPUTS_IN_ACTIVATIONS) AI_ALIGNED(4) ai_i8 data_in_1[AI_NETWORK_IN_1_SIZE_BYTES]; ai_i8* data_ins[AI_NETWORK_IN_NUM] = { data_in_1 }; #else ai_i8* data_ins[AI_NETWORK_IN_NUM] = { NULL }; #endif #if !defined(AI_NETWORK_OUTPUTS_IN_ACTIVATIONS) AI_ALIGNED(4) ai_i8 data_out_1[AI_NETWORK_OUT_1_SIZE_BYTES]; ai_i8* data_outs[AI_NETWORK_OUT_NUM] = { data_out_1 }; #else ai_i8* data_outs[AI_NETWORK_OUT_NUM] = { NULL }; #endif /* Activations buffers -------------------------------------------------------*/ AI_ALIGNED(32) static uint8_t pool0[AI_NETWORK_DATA_ACTIVATION_1_SIZE]; ai_handle data_activations0[] = {pool0}; /* AI objects ----------------------------------------------------------------*/ static ai_handle network = AI_HANDLE_NULL; static ai_buffer* ai_input; static ai_buffer* ai_output; static void ai_log_err(const ai_error err, const char *fct) { /* USER CODE BEGIN log */ if (fct) printf("TEMPLATE - Error (%s) - type=0x%02x code=0x%02x\r\n", fct, err.type, err.code); else printf("TEMPLATE - Error - type=0x%02x code=0x%02x\r\n", err.type, err.code); do {} while (1); /* USER CODE END log */ } static int ai_boostrap(ai_handle *act_addr) { ai_error err; /* Create and initialize an instance of the model */ err = ai_network_create_and_init(&network, act_addr, NULL); if (err.type != AI_ERROR_NONE) { ai_log_err(err, "ai_network_create_and_init"); return -1; } ai_input = ai_network_inputs_get(network, NULL); ai_output = ai_network_outputs_get(network, NULL); printf("input[0] : (%d, %d, %d)\r\n", AI_BUFFER_SHAPE_ELEM(ai_input, AI_SHAPE_HEIGHT), AI_BUFFER_SHAPE_ELEM(ai_input, AI_SHAPE_WIDTH), AI_BUFFER_SHAPE_ELEM(ai_input, AI_SHAPE_CHANNEL)); printf("output[0] : (%d, %d, %d)\r\n", AI_BUFFER_SHAPE_ELEM(ai_output, AI_SHAPE_HEIGHT), AI_BUFFER_SHAPE_ELEM(ai_output, AI_SHAPE_WIDTH), AI_BUFFER_SHAPE_ELEM(ai_output, AI_SHAPE_CHANNEL)); //my ai_input[0].data = AI_HANDLE_PTR(data_ins); ai_output[0].data = AI_HANDLE_PTR(data_outs); //my #if defined(AI_NETWORK_INPUTS_IN_ACTIVATIONS) /* In the case where "--allocate-inputs" option is used, memory buffer can be * used from the activations buffer. This is not mandatory. */ for (int idx=0; idx < AI_NETWORK_IN_NUM; idx++) { data_ins[idx] = ai_input[idx].data; } #else for (int idx=0; idx < AI_NETWORK_IN_NUM; idx++) { ai_input[idx].data = data_ins[idx]; } #endif #if defined(AI_NETWORK_OUTPUTS_IN_ACTIVATIONS) /* In the case where "--allocate-outputs" option is used, memory buffer can be * used from the activations buffer. This is no mandatory. */ for (int idx=0; idx < AI_NETWORK_OUT_NUM; idx++) { data_outs[idx] = ai_output[idx].data; } #else for (int idx=0; idx < AI_NETWORK_OUT_NUM; idx++) { ai_output[idx].data = data_outs[idx]; } #endif return 0; } static int ai_run(void) { ai_i32 batch; batch = ai_network_run(network, ai_input, ai_output); if (batch != 1) { ai_log_err(ai_network_get_error(network), "ai_network_run"); return -1; } return 0; } /* USER CODE BEGIN 2 */ int acquire_and_process_data(ai_i8* data[]) { /* fill the inputs of the c-model for (int idx=0; idx < AI_NETWORK_IN_NUM; idx++ ) { data[idx] = .... } */ for (int idx=0; idx < AI_NETWORK_IN_NUM; idx++ ) { data[idx] = daisy; } return 0; return 0; } int post_process(ai_i8* data[]) { /* process the predictions for (int idx=0; idx < AI_NETWORK_OUT_NUM; idx++ ) { data[idx] = .... } */ printf("Result-1\r\n");//My printf("Result1: %f \r\n",*((float *)(data[0])+0));//My printf("Result2: %f \r\n",*((float *)(data[0])+1));//My printf("Result3: %f \r\n",*((float *)(data[0])+2));//My printf("Result4: %f \r\n",*((float *)(data[0])+3));//My printf("Result5: %f \r\n",*((float *)(data[0])+4));//My while(1){}; return 0; } /* USER CODE END 2 */ /* Entry points --------------------------------------------------------------*/ void MX_X_CUBE_AI_Init(void) { /* USER CODE BEGIN 5 */ printf("\r\nTEMPLATE - initialization\r\n"); ai_boostrap(data_activations0); /* USER CODE END 5 */ } void MX_X_CUBE_AI_Process(void) { /* USER CODE BEGIN 6 */ int res = -1; printf("TEMPLATE - run - main loop\r\n"); if (network) { do { /* 1 - acquire and pre-process input data */ res = acquire_and_process_data(data_ins); printf("1\r\n"); /* 2 - process the data - call inference engine */ if (res == 0) res = ai_run(); printf("2\r\n"); printf("res after run:%d\r\n",res); /* 3- post-process the predictions */ if (res == 0) res = post_process(data_outs); printf("3\r\n"); } while (res==0); } if (res) { ai_error err = {AI_ERROR_INVALID_STATE, AI_ERROR_CODE_NETWORK}; ai_log_err(err, "Process has FAILED"); } /* USER CODE END 6 */ } #ifdef __cplusplus } #endif