/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2023 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" #include "app_x-cube-ai.h" #include "stdio.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ CRC_HandleTypeDef hcrc; DCMI_HandleTypeDef hdcmi; OSPI_HandleTypeDef hospi1; RTC_HandleTypeDef hrtc; UART_HandleTypeDef huart1; PCD_HandleTypeDef hpcd_USB_OTG_HS; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_USART1_UART_Init(void); static void MX_DCMI_Init(void); static void MX_OCTOSPI1_Init(void); static void MX_RTC_Init(void); static void MX_CRC_Init(void); static void MX_USB_OTG_HS_PCD_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* Enable I-Cache---------------------------------------------------------*/ SCB_EnableICache(); /* Enable D-Cache---------------------------------------------------------*/ SCB_EnableDCache(); /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_USART1_UART_Init(); MX_DCMI_Init(); MX_OCTOSPI1_Init(); MX_RTC_Init(); MX_CRC_Init(); MX_USB_OTG_HS_PCD_Init(); MX_X_CUBE_AI_Init(); /* USER CODE BEGIN 2 */ /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ MX_X_CUBE_AI_Process(); /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Supply configuration update enable */ HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY); /** Configure the main internal regulator output voltage */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0); while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {} /** Configure LSE Drive Capability */ HAL_PWR_EnableBkUpAccess(); __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW); /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_HSE |RCC_OSCILLATORTYPE_LSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.LSEState = RCC_LSE_ON; RCC_OscInitStruct.HSI48State = RCC_HSI48_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 10; RCC_OscInitStruct.PLL.PLLN = 220; RCC_OscInitStruct.PLL.PLLP = 1; RCC_OscInitStruct.PLL.PLLQ = 2; RCC_OscInitStruct.PLL.PLLR = 2; RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_1; RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE; RCC_OscInitStruct.PLL.PLLFRACN = 0; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2; RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2; RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK) { Error_Handler(); } } /** * @brief CRC Initialization Function * @param None * @retval None */ static void MX_CRC_Init(void) { /* USER CODE BEGIN CRC_Init 0 */ /* USER CODE END CRC_Init 0 */ /* USER CODE BEGIN CRC_Init 1 */ /* USER CODE END CRC_Init 1 */ hcrc.Instance = CRC; hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE; hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE; hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE; hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE; hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES; if (HAL_CRC_Init(&hcrc) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN CRC_Init 2 */ /* USER CODE END CRC_Init 2 */ } /** * @brief DCMI Initialization Function * @param None * @retval None */ static void MX_DCMI_Init(void) { /* USER CODE BEGIN DCMI_Init 0 */ /* USER CODE END DCMI_Init 0 */ /* USER CODE BEGIN DCMI_Init 1 */ /* USER CODE END DCMI_Init 1 */ hdcmi.Instance = DCMI; hdcmi.Init.SynchroMode = DCMI_SYNCHRO_HARDWARE; hdcmi.Init.PCKPolarity = DCMI_PCKPOLARITY_RISING; hdcmi.Init.VSPolarity = DCMI_VSPOLARITY_LOW; hdcmi.Init.HSPolarity = DCMI_HSPOLARITY_LOW; hdcmi.Init.CaptureRate = DCMI_CR_ALL_FRAME; hdcmi.Init.ExtendedDataMode = DCMI_EXTEND_DATA_8B; hdcmi.Init.JPEGMode = DCMI_JPEG_DISABLE; hdcmi.Init.ByteSelectMode = DCMI_BSM_ALL; hdcmi.Init.ByteSelectStart = DCMI_OEBS_ODD; hdcmi.Init.LineSelectMode = DCMI_LSM_ALL; hdcmi.Init.LineSelectStart = DCMI_OELS_ODD; if (HAL_DCMI_Init(&hdcmi) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN DCMI_Init 2 */ /* USER CODE END DCMI_Init 2 */ } /** * @brief OCTOSPI1 Initialization Function * @param None * @retval None */ static void MX_OCTOSPI1_Init(void) { /* USER CODE BEGIN OCTOSPI1_Init 0 */ /* USER CODE END OCTOSPI1_Init 0 */ OSPIM_CfgTypeDef sOspiManagerCfg = {0}; /* USER CODE BEGIN OCTOSPI1_Init 1 */ /* USER CODE END OCTOSPI1_Init 1 */ /* OCTOSPI1 parameter configuration*/ hospi1.Instance = OCTOSPI1; hospi1.Init.FifoThreshold = 8; hospi1.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE; hospi1.Init.MemoryType = HAL_OSPI_MEMTYPE_MICRON; hospi1.Init.DeviceSize = 23; hospi1.Init.ChipSelectHighTime = 1; hospi1.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE; hospi1.Init.ClockMode = HAL_OSPI_CLOCK_MODE_3; hospi1.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED; hospi1.Init.ClockPrescaler = 2; hospi1.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_HALFCYCLE; hospi1.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_DISABLE; hospi1.Init.ChipSelectBoundary = 0; hospi1.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_BYPASSED; hospi1.Init.MaxTran = 0; hospi1.Init.Refresh = 0; if (HAL_OSPI_Init(&hospi1) != HAL_OK) { Error_Handler(); } sOspiManagerCfg.ClkPort = 1; sOspiManagerCfg.NCSPort = 1; sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_1_LOW; if (HAL_OSPIM_Config(&hospi1, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN OCTOSPI1_Init 2 */ /* USER CODE END OCTOSPI1_Init 2 */ } /** * @brief RTC Initialization Function * @param None * @retval None */ static void MX_RTC_Init(void) { /* USER CODE BEGIN RTC_Init 0 */ /* USER CODE END RTC_Init 0 */ /* USER CODE BEGIN RTC_Init 1 */ /* USER CODE END RTC_Init 1 */ /** Initialize RTC Only */ hrtc.Instance = RTC; hrtc.Init.HourFormat = RTC_HOURFORMAT_24; hrtc.Init.AsynchPrediv = 127; hrtc.Init.SynchPrediv = 255; hrtc.Init.OutPut = RTC_OUTPUT_DISABLE; hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH; hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN; hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE; if (HAL_RTC_Init(&hrtc) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN RTC_Init 2 */ /* USER CODE END RTC_Init 2 */ } /** * @brief USART1 Initialization Function * @param None * @retval None */ static void MX_USART1_UART_Init(void) { /* USER CODE BEGIN USART1_Init 0 */ /* USER CODE END USART1_Init 0 */ /* USER CODE BEGIN USART1_Init 1 */ /* USER CODE END USART1_Init 1 */ huart1.Instance = USART1; huart1.Init.BaudRate = 115200; huart1.Init.WordLength = UART_WORDLENGTH_8B; huart1.Init.StopBits = UART_STOPBITS_1; huart1.Init.Parity = UART_PARITY_NONE; huart1.Init.Mode = UART_MODE_TX_RX; huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart1.Init.OverSampling = UART_OVERSAMPLING_16; huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1; huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart1) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_DisableFifoMode(&huart1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART1_Init 2 */ /* USER CODE END USART1_Init 2 */ } int fputc(int ch, FILE *f) { HAL_UART_Transmit(&huart1, (uint8_t *)&ch, 1, 100); // 发送单字节数据 return (ch); } /** * @brief USB_OTG_HS Initialization Function * @param None * @retval None */ static void MX_USB_OTG_HS_PCD_Init(void) { /* USER CODE BEGIN USB_OTG_HS_Init 0 */ /* USER CODE END USB_OTG_HS_Init 0 */ /* USER CODE BEGIN USB_OTG_HS_Init 1 */ /* USER CODE END USB_OTG_HS_Init 1 */ hpcd_USB_OTG_HS.Instance = USB_OTG_HS; hpcd_USB_OTG_HS.Init.dev_endpoints = 9; hpcd_USB_OTG_HS.Init.speed = PCD_SPEED_FULL; hpcd_USB_OTG_HS.Init.dma_enable = DISABLE; hpcd_USB_OTG_HS.Init.phy_itface = USB_OTG_EMBEDDED_PHY; hpcd_USB_OTG_HS.Init.Sof_enable = DISABLE; hpcd_USB_OTG_HS.Init.low_power_enable = DISABLE; hpcd_USB_OTG_HS.Init.lpm_enable = DISABLE; hpcd_USB_OTG_HS.Init.vbus_sensing_enable = DISABLE; hpcd_USB_OTG_HS.Init.use_dedicated_ep1 = DISABLE; hpcd_USB_OTG_HS.Init.use_external_vbus = DISABLE; if (HAL_PCD_Init(&hpcd_USB_OTG_HS) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USB_OTG_HS_Init 2 */ /* USER CODE END USB_OTG_HS_Init 2 */ } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOE_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOF_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOG_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE(); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */