User Activity

I am curious about these parameters,I don`t konw where they are used.These are auto generated by following the official guide, but if I want to build a project with x-cube-ai and CubeMX my own and still use the model from model zoo, how shoul i deal ...
i get two defferent results with O0 and O2 optimizationO0 result O2 resultBut I think the result of O2 is more like right because the label is daisy.Should I always open O2 optimization? 
I meet that when follow func is in its second  loop And I find the value of var 'batch' is not 1 in the second loop,Why?  
This is the model i use(through X cube ai 8.1.0)By annalyze it ,the output should be float as belowBut the auto generated code declare it as ai_i8,why?and I can`t get result in the following way,I don`t konw the reason Because of the limits ,I can on...
Kudos from