2024-07-08 06:36 AM - last edited on 2024-07-23 08:38 AM by Amel NASRI
Hello ST team,
I have logged raw data by using hsdatalog_GUI.py in STM32CubeFunctionPack_DATALOG2_V2.1.1 from STEVAL-STWINKT1b board to PC and seen the FFT diagram in GUI. The acquired raw data was saved locally in an automatically generated folder. After that I tried to plot FFT figure by activing the command hsdatalog_plot.py -ft. However, figures it plot are all in time domain. Figures are attached below. What I expected is the power density spectrum over a frequency band.
2024-07-25 07:40 AM
Hello @JW1
The figure you attached is the Power Spectral Density of the accelerometer data, so it is not true that all figures are in time domain.
HSDPython SDK supports PSD calculation for microphones and accelerometers only.
What are you expecting for? Am I misunderstanding your question?
Best regards
Simone