2024-07-28 05:49 AM
I am validating a classification model on STM32H745-DISC0 board.
The validation is successful but id does not show any accuracy related parameter.
It shows all the parameters except accuracy.
rmse | Mae | L2r | mean | std |
Ritesh
2024-07-29 03:59 AM
Hello,
The tool shows accuracy (acc column) means "Classification accuracy". If it is not displayed, it means we were not able to detect your model as a classifier. You can still force this flag with '--classifier' or through the "Advanced Settings" in STM32CubeMX / X-CUBE-AI.
From the embedded documentation:
"
For classifier model type, Classification accuracy is what we usually mean, when the term accuracy is used. ACC is the ratio between of correct predictions to the total number of inputs. This indicator evaluates the performance of the classifier model, if a regressor type is passed, the ACC is NOT calculated and n.a. value is reported
"
Best regards,
Yanis
2024-07-31 04:33 AM
Thanks for the reply.
I forced the model as classifier, but still it does not show the accuracy.
Ritesh