2024-07-28 5:49 AM
I am validating a classification model on STM32H745-DISC0 board.
The validation is successful but id does not show any accuracy related parameter.
It shows all the parameters except accuracy.
rmse | Mae | L2r | mean | std |
Ritesh
Solved! Go to Solution.
2024-08-01 1:28 AM
Hello,
I assume here you are refering to the validation result in X-CUBE-AI interface in STM32CubeMX.
While doing the validation, could you verify if you have something like these rows in the textual output:
Computing the metrics...
Cross accuracy report #1 (reference vs C-model)
----------------------------------------------------------------------------------------------------
notes: - the output of the reference model is used as ground truth/reference value
- 10 samples (5 items per sample)
acc=100.00%, rmse=0.000000153, mae=0.000000065, l2r=0.000000396, nse=1.000, cos=1.000
5 classes (10 samples)
---------------------------------
C0 0 . . . .
C1 . 0 . . .
C2 . . 0 . .
C3 . . . 8 .
C4 . . . . 2
Evaluation report (summary)
-------------------------------------------------------------------------------------------------------------------------------------------
Output acc rmse mae l2r mean std nse cos tensor
-------------------------------------------------------------------------------------------------------------------------------------------
X-cross #1 100.00% 0.0000002 0.0000001 0.0000004 -0.0000000 0.0000002 1.0000000 1.0000000 activation_3, (5,), m_id=[5]
-------------------------------------------------------------------------------------------------------------------------------------------
acc : Classification accuracy (all classes)
rmse : Root Mean Squared Error
mae : Mean Absolute Error
l2r : L2 relative error
nse : Nash-Sutcliffe efficiency criteria, bigger is better, best=1, range=(-inf, 1]
cos : COsine Similarity, bigger is better, best=1, range=(0, 1]
You should have at least one row (X-cross #<n> where n is the output index).
Best regards,
Yanis
2024-07-29 3:59 AM
Hello,
The tool shows accuracy (acc column) means "Classification accuracy". If it is not displayed, it means we were not able to detect your model as a classifier. You can still force this flag with '--classifier' or through the "Advanced Settings" in STM32CubeMX / X-CUBE-AI.
From the embedded documentation:
"
For classifier model type, Classification accuracy is what we usually mean, when the term accuracy is used. ACC is the ratio between of correct predictions to the total number of inputs. This indicator evaluates the performance of the classifier model, if a regressor type is passed, the ACC is NOT calculated and n.a. value is reported
"
Best regards,
Yanis
2024-07-31 4:33 AM
Thanks for the reply.
I forced the model as classifier, but still it does not show the accuracy.
Ritesh
2024-08-01 1:28 AM
Hello,
I assume here you are refering to the validation result in X-CUBE-AI interface in STM32CubeMX.
While doing the validation, could you verify if you have something like these rows in the textual output:
Computing the metrics...
Cross accuracy report #1 (reference vs C-model)
----------------------------------------------------------------------------------------------------
notes: - the output of the reference model is used as ground truth/reference value
- 10 samples (5 items per sample)
acc=100.00%, rmse=0.000000153, mae=0.000000065, l2r=0.000000396, nse=1.000, cos=1.000
5 classes (10 samples)
---------------------------------
C0 0 . . . .
C1 . 0 . . .
C2 . . 0 . .
C3 . . . 8 .
C4 . . . . 2
Evaluation report (summary)
-------------------------------------------------------------------------------------------------------------------------------------------
Output acc rmse mae l2r mean std nse cos tensor
-------------------------------------------------------------------------------------------------------------------------------------------
X-cross #1 100.00% 0.0000002 0.0000001 0.0000004 -0.0000000 0.0000002 1.0000000 1.0000000 activation_3, (5,), m_id=[5]
-------------------------------------------------------------------------------------------------------------------------------------------
acc : Classification accuracy (all classes)
rmse : Root Mean Squared Error
mae : Mean Absolute Error
l2r : L2 relative error
nse : Nash-Sutcliffe efficiency criteria, bigger is better, best=1, range=(-inf, 1]
cos : COsine Similarity, bigger is better, best=1, range=(0, 1]
You should have at least one row (X-cross #<n> where n is the output index).
Best regards,
Yanis
2024-08-01 8:06 AM
Except accuracy it shows all the parameters. I will try with a different classification model.
Thanks
Ritesh
2024-08-03 1:35 PM
Could you provide the NN model that you are using for the test purpose as I used the 3-4 different classification models and with none of them I got the accuracy during validation.
Ritesh
2024-08-04 11:18 PM - edited 2024-08-04 11:18 PM
Hello,
For my example I use a simple model but I can reproduce this accuracy using models from our STM32 Model Zoo: https://github.com/STMicroelectronics/stm32ai-modelzoo/tree/main/image_classification/pretrained_models/fdmobilenet/ST_pretrainedmodel_public_dataset
Evaluation report (summary)
--------------------------------------------------------------------------------------------------------------------------------------------
Output acc rmse mae l2r mean std nse cos tensor
--------------------------------------------------------------------------------------------------------------------------------------------
X-cross #1 100.00% 0.0418388 0.0187500 0.1083516 0.0003125 0.0422624 0.9842321 0.9941229 conversion_35, (5,), m_id=[35]
--------------------------------------------------------------------------------------------------------------------------------------------
Is it possible to also share your model to see if I can reproduce it ?
Best regards,
Yanis
2024-08-13 11:42 PM
How to provide images as a validation input.