2021-07-18 9:04 AM
Hello everyone,
I am trying to deploy ML model to microcontrollers and I have two boards of STM32L4R9I-Discovery and STM32H7B3I-Discovery. The experiments and related results are shown below:
I use TFLite Micro and STM32Cube.AI runtime to profile my ML model and then compile on two different boards. The hardware resource related to these two boards are provided and STM32H7B3I is a bigger one. However, it's strange that I can successively get the results on smaller board (STM32L4R9I) but build fail on a bigger one (STM32H7B3I) with the following error:
.../arm-none-eabi/bin/ld.exe: *****.elf section `.bss' will not fit in region `RAM'
.../arm-none-eabi/bin/ld.exe: region `RAM' overflowed by 251112 bytes
Could anyone provide some suggestions about how to address this issue? Thank you very much.
Best regards,
Jeff
Solved! Go to Solution.
2021-07-19 7:31 AM
I'm not familiar with STM32Cube.AI. It is possible it requires two separate sections here for some reason. If it were a regular project, you could simply swap the names of those two.
> I have tried to increase the length of RAM in "STM32H7B3LIHXQ_RAM.ld" and then built again, but the length of RAM in "STM32H7B3I_ST_MCU2.map" doesn't change.
Are you sure it's using that linker script? Look in the command line output when you build to see what it uses. The default in many cases is the FLASH linker script.
2021-07-18 5:47 PM
Go into the STM32H7B3I linker file and figure out what section "RAM" points to. You may be able to change the size by locating it somewhere else. See the memory map in the refence manual for available spaces, specifically SRAM1-3.
2021-07-18 9:24 PM
Hello TDK,
Thank you very much for your reply. I am a novice of microcontrollers. Based on your suggestion, I have checked "STM32H7B3LIHXQ_RAM.ld" and found the following information:
MEMORY
{
RAM_EXEC (xrw) : ORIGIN = 0x24000000, LENGTH = 1024K
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
AHB_SRAM (xrw) : ORIGIN = 0x30000000, LENGTH = 128K
}
The part of RAM is actually not enough. Based on the reference manual, SRAM1-3 have 256KB, 384KB and 384KB, respectively, and I guess it is the part of RAM_EXEC. And I have also checked "STM32H7B3I_ST_MCU2.map" and got the following information:
Memory Configuration
Name Origin Length Attributes
FLASH 0x08000000 0x00200000 xr
RAM 0x20000000 0x00020000 xrw
AXI_SRAM 0x24000000 0x00100000 xrw
AHB_SRAM 0x30000000 0x00020000 xrw
*default* 0x00000000 0xffffffff
It is strange that the name of RAM_EXEC is changed to AXI_SRAM. I have tried to increase the length of RAM in "STM32H7B3LIHXQ_RAM.ld" and then built again, but the length of RAM in "STM32H7B3I_ST_MCU2.map" doesn't change.
Could you provide more information about how to address this issue? I also attach these two files as references. Thank you very much!
Best regards,
Jeff
2021-07-19 7:31 AM
I'm not familiar with STM32Cube.AI. It is possible it requires two separate sections here for some reason. If it were a regular project, you could simply swap the names of those two.
> I have tried to increase the length of RAM in "STM32H7B3LIHXQ_RAM.ld" and then built again, but the length of RAM in "STM32H7B3I_ST_MCU2.map" doesn't change.
Are you sure it's using that linker script? Look in the command line output when you build to see what it uses. The default in many cases is the FLASH linker script.
2021-07-19 1:34 PM
Hi TDK,
You are amazing. After checking, it actually uses the FLASH linker script. And after I swap the names, it is successfully built.
Thank you very much for your useful instructions!
Best regards,
Jeff