Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Unresolved inclusion - SPC5Studio 6.0

I have just installed SPC5Studio 6.0 and I have opened GTM DPLL Test Application. I am getting the "Unresolved inclusion" error for#include "components.h"#include <build/mcs/mcs0.h>How do I resolve this? I don't seem to have any folders like the ones...

JHoll.1 by Associate II
  • 2868 Views
  • 4 replies
  • 0 kudos

Where to download SPC570S-DISP JTAG Driver?

Hello ST CommunityI have got the SPC570S-DISP: Discovery Evaluation Board,I want to test it with a sample application from the library, but My computer has no driver, where to download it?I have no experience with SPC5 MCU, I just know about STM32 MC...

0693W000007EGGuQAO.jpg 0693W000007EGGpQAO.jpg
MKham.1 by Associate
  • 1219 Views
  • 1 replies
  • 0 kudos

Phase Shift and Dead Time with SPC574S

Hello,I can generate 4 PWMs ( 2 x Complementary Pair) with dead-time but I want to add phase-shift to a complementary pair which is one of them. How can I implement this?Best Regards

Msert.1 by Associate III
  • 1087 Views
  • 1 replies
  • 0 kudos

Resolved! SPC5 code call from flash to RAM

Hi,I've got the latest SPC5Studio 6 with all updates (gcc4.9.4) and testing on the SPC560D40L1 chip with the discovery board. So core is e200z0h VLE.I want to manipulate the flash in my app so I need to call some code from the RAM. I added the necess...

MDupo.1 by Associate
  • 1896 Views
  • 2 replies
  • 0 kudos