2023-05-22 12:08 AM
2023-05-22 7:09 AM
2023-05-22 7:09 AM
it seems to be a coredump issue.
Please check PC, R14 and R13
2023-05-22 8:05 AM
In addition to Erwan's suggestion check also MCSR register and if MAV field (bit-19) is set then register MCAR contains the address of the fault.
Regards.