cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, when I use SPC5Studio software to program the SPC582B microcontroller, how can I set the data sent by SPI communication through SPC5Studio ?

Bwang.3
Associate III

Hello, when I use SPC5Studio software to program the SPC582B microcontroller, how can I set the data sent by SPI communication through SPC5Studio? Because I cannot find the SPI module's menu or options for setting the content of data sent in the SPC5Studio software! Can you tell me!

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
ODOUV.1
ST Employee

Hello,

import and look at this Chorus 1M example : "SPC582Bxx_RLA DSPI Test Application for Discovery"

Best regards.

If I want to use DSPI to send two data 0x26 and 0x69, where should I fill in these two data? I couldn't find an option in the "SPC582Bxx_RLA DSPI Test Application for Discovery" application to place the two data I need to send!

ODOUV.1
ST Employee

You have to use the SPD driver like in the example

start the driver:

spi_lld_start(&SPID1, &spi_config_low_speed);

put your two bytes in txbuf:

txbuf[0] = 0x26;

txbuf[1] = 0x69;

send these 2 bytes through API:

spi_lld_send(&SPID1, 2, txbuf);

then stop the driver:

spi_lld_stop(&SPID1);