cancel
Showing results for 
Search instead for 
Did you mean: 

TESEO-LIV4F Trouble using $PSTMEPHEM

JCharette
Associate III

Hi all, 

We're having trouble getting the module to respond to the message "$PSTMEPHEM" We're attempting to upload ephemeris data but the module is ignoring the message, ie: the module is not responding with either "PSTMEPHEMOK" or '"PSTMEPHEMERROR" 

To help debug this, we did the following,

  1. We used 'PSTMDUMPEPHEMS' to get emphemerides and ensure our formatting is correct, and load them into an array.
  2. We then cold-start the module and use "PSTMINITGPS" to initialize the approximate time and position, to which we do receive a 'PSTMINITGPSOK' in response.
  3. Then we try to upload one of the ephemeris strings (received in step 1), but we get no response, OK or ERROR

We are able to get/set parameters, init time and position, and dump ephemeris data just fine, but we can't seem to get a response to the 'PSTMEPHEM' message,  try as we might.

Any help in this matter would be greatly appreciated.

Thank you in advance,

-Jake

7 REPLIES 7
GalaxyQuest
ST Employee

Hi Jake,

I checked with our development engineers. In LIV4F, we have not implemented PSTMEPHEM. We will implement this in our next release.

Have you looked at our LIV3FL module? This is pin-to-pin with LIV4F and can support EPHEM injection. LIV3FL also has STAGPS built-in which STs proprietary Assisted GNSS. You would not need to explicitly inject EPH and we would do the ephermeris prediction internally.

 

 

 

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

GalaxyQuest, thank you for checking into this for me.  Do you mean in the next firmware release for the LIV4F, you will be including PSTMEPHEM, or in the next LIV# module release?  If it is a new firmware release, do you have any estimate of when it will be available?  We have previously considered the LIV3FL, but decided on the LIV4F due to the increased accuracy and access to the L5 band.

 

Thanks again, 

-Jake

Hi Jake,

I would need to check on this and get back.

Thanks,

George


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
JCharette
Associate III

Hi, 

I was wondering if there was any update on this?

Thank you, 

-Jake

Hi Jake,

Our applications team is working to add this. Please give us an additional couple of weeks for implementation and testing.

Thank you.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

George, 

Oh, awesome!  Thank you, this is very much appreciated!

-Jake

Hi Jake,

Just an FYI, we will be releasing a new version of firmware with $PSTMEPHEM supported very soon. This has been implemented.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.