cancel
Showing results for 
Search instead for 
Did you mean: 

Adding breakpoint and debugging using UDE STK 2021

nanda_kishore
Associate

Hello everyone,

I have been flashing the code written in AutDevKit Studio 2.4.0 using UDE STK 2021 for the AEK-AUD-C1D9031, which uses the SPC582B60E1 MCU. I want to start debugging the code line by line using breakpoints.

Currently, I have the option to add breakpoints in AutDevKit Studio, but it is of no use since I am flashing the code with UDE STK 2021.

Could someone guide me on how to add breakpoints in UDE STK 2021? Also, how can I add variables to the watch window?

I referred to the manual I attached but couldn’t figure out the exact steps to add breakpoints or watch variables in the program shown in UDE STK 2021.

1 ACCEPTED SOLUTION

Accepted Solutions
Max VIZZINI
ST Employee
1 REPLY 1
Max VIZZINI
ST Employee

Hi,

Basic info can be found here:

Part 7 - AutoDevKit™ detailed tutorial: Debug and release of firmware created with AutoDevKit™

Best Regards,

AutoDevKit Team