cancel
Showing results for 
Search instead for 
Did you mean: 

TSV6392A SPICE model and output

kaushalyas
Associate

Hi,

1. Is there a SPICE model available for this part?

2. Is the output open-drain or push-pull?

 

Cheers,

Kay

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
LCE
Principal

1. Is there a SPICE model available for this part?

It seems there's only the eDesignSuite link, I just tried it and that's quite useless, because TSV6392A can't be selected.
BUT the datasheet says something about a macro model...

> 2. Is the output open-drain or push-pull?

It's declared as an opamp, so that's usually push-pull.

Pierre SENNEQUIER
ST Employee

Hi Kay,

 

  Please find it attached.

As mentioned by LCE, yes this is a rail to rail op amp.

 

   Have a nice day,

 

Pierre

In order to give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.