2017-07-20 05:13 AM
Hello Community,
Does the SAI sub-block clock source matter when it is in Synchronous Slave mode with the other sub-block? In other words, should the two sub-blocks have the same clock source?Thank you.
2017-09-23 12:10 PM
Hello,
To use two block SAI working synchronously, you need to configure the first block as an asynchronous master and the other one as a synchronous slave. Then, The two blocks will share the FS ,BCLK and MCLK lines. And each one will have its own data line.