cancel
Showing results for 
Search instead for 
Did you mean: 

Gain of TS922

TomRett
Associate III

Hi, im trying to find out the gain from the TS922EIJT used inside the STEVAL-STWINKT1B evaluation board. Here is where the opamp is used.

TomRett_0-1701243816881.png

So far, i have simulated the schematic using LTSpice and got a gain of -80 dB (see attached screenshot of the circuit)

TomRett_1-1701243997154.png

Is this gain correct? I saw the open loop characteristics inside the documentation of this opamp and this here looks nothing like it. Since im calibrating my system i have to know the gain of this opamp. Is the unit in dBV or dB? And if it is in dBV, is it normalized to dB re 1V/Pa?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
AScha.3
Chief III

dont know, what you simulate... :)

the opamp has 100k/4k7 feedback , ~ 20x , or 26 dB .  ( dB is used for gain ; dBV for Voltage )

If you feel a post has answered your question, please click "Accept as Solution".
LCE
Principal

AScha.3 got it.

Anyway, I think I've seen some years ago that drawing opamps like this (square with pins) is IEEE-something conform, but honestly, it is TERRIBLE! It took more than the usual one glance to see it's just a voltage follower and an non-inverting (edited) amp... ;)
Getting old... (?)

TomRett
Associate III

My calibration signal produces 94 dBSPL @1kHz which causes this mic to produce a -38dBV +-1. This number (-38dBV) is then added with the gain of the opamp (26 dB) which is -12 dBV +-1 (at this point that number irritates me). However, this is not what im measuring with the STWINKT1B-EVAL. Instead i get a peak at approx. -51 dBV which should be -38 dBV. A difference of approx. 13 dBV. Am i missing something that i have to consider in order to get the -38 dBV? 

>Am i missing something

yes - check with a scope , what you have really there !

1. the mic level...see ~  10mV ?

2. after amp, at cpu pin : see ~ 200 mV ?

If you feel a post has answered your question, please click "Accept as Solution".