2020-08-24 08:41 PM
I have a diode that I am trying to identify. Its markings are:
ST e3
ZTTH (the 'Z' is backward)
112
230
Anybody know what it is and what can be used to replace it?
2020-08-24 09:02 PM
On closer inspection it has a 'G' between the STe3 line and the ZTTH line
ST e3
G
ZTTH (the 'Z' is backward)
112
230
2020-09-01 04:01 AM
This one STTH112 ?
2020-09-01 06:38 AM
Could be. I found a schematic for similar UPS (slightly different model) and they had a 1N4003 in the same location on the circuit so I used a 1N4007, which I have plenty to hand, and the unit is now working. The MOSFETs were also shot as was the fuse, the diode was the only component I wasn't sure about.
Some of these UPS have Schottky diodes in the switchmode section and will not run properly with a regular diode so I was worried about that. But upon testing the diode was in the regular diode range so that gave me confidence.
Thanks for that, I'll file the datasheet for next time 🙂