cancel
Showing results for 
Search instead for 
Did you mean: 

How to build a .dfu file from an STM32CubeIDE project?

CDew.1
Associate III

The code compiles and works on the Nucleo H743ZI2.

The contents of the Debug directory are:

$ ls -lA Debug/

total 3132

drwxrwxr-x 4 chris chris   4096 Jun 19 11:51 Core

drwxrwxr-x 3 chris chris   4096 Jun 19 11:51 Drivers

-rwxrwxr-x 1 chris chris  30384 Jun 19 11:59 h743-dfutest.bin

-rwxrwxr-x 1 chris chris 1999356 Jun 19 11:59 h743-dfutest.elf

-rw-rw-r-- 1 chris chris 704111 Jun 19 11:59 h743-dfutest.list

-rw-rw-r-- 1 chris chris 533170 Jun 19 11:59 h743-dfutest.map

-rw-rw-r-- 1 chris chris   2028 Jun 19 11:59 makefile

-rw-rw-r-- 1 chris chris   1596 Jun 19 11:59 objects.list

-rw-rw-r-- 1 chris chris    231 Jun 19 11:51 objects.mk

-rw-rw-r-- 1 chris chris    507 Jun 19 11:59 sources.mk

How do I make a h743-dfutest.dfu file from this project, that I could use with dfuse? http://dfu-util.gnumonks.org/dfuse.html

0 REPLIES 0