Associate II
Jan 10, 2020 2:34 PM UTC
Question
config OPAMP in non-inverting configuration with the output of opamp connected to ADC: is it possible?
- 2 replies
- 2992 views
Good morning,
i' m working with stm32g4 and for
my application i need use internal opamp in non- inverting configuration with
external resistor how show the figure below (figure form AN5306).

I don’t understand if is possible connect the output of opamp to ADC when i use external resistors to set the gain. Reading AN5306 seems that i can choose only one option:
OPAINTOEN = 0 connect the output of opamp to Vout.
Or OPAINTOEN = 1 connect the output of opamp to ADC.
How can i connect the output of opamp to ADC and use it in non-inverting configuration with external resistor?
Thanks in advance