cancel
Showing results for 
Search instead for 
Did you mean: 

ADC common registers inaccessible?

JCtib
Associate II

Hello,

i have a problem. I cant write any values into ADC12 common configuration register CCR. It is not possible if ADCs are disabled (as recomended in ref.man.) either they are enabled. I tried to change it using LL functions or CMSIS registers access (ADC12_COMMON->CCR = .... ) and both methods are not success.

Do you have any advice?

Tahnk you so much.

George

4 REPLIES 4
JCtib
Associate II

Either in SFRs view it is not possible to change them as in another registers.

0690X00000BuVb9QAF.png

Bassett.David
Senior

I seem to recall finding address errors in the .svd file for the common registers. I don't have my notes handy at the moment, but try comparing the debugger's address for the registers with those of the data sheet. Good luck!

Dave

Bassett.David
Senior

Notes located:

ADC12_Common is 0x50000200 in .svd, should be 0x50000300

ADC5 is 0x50000600 in .svd, should be 0x50000200

Please verify before using.

Regards,

Dave

JCtib
Associate II

Hello,

I dont know which files i should compare, but nevermind.

I can confirm, that this issue is caused only by debugger problems, dual DMA transfer is working properly.

Thank you for your advice, in case i need debug this, i will check .svd file.

Best regards,

George