cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743ZI NUCLEO 144 & LWIP - Can't Ping The Board

CodesMagic
Associate II

Hope all is going well. I'm trying to ping STM32H743ZI NUCLEO 144 using LWIP middle-ware. Code generated by CubeMX.

  • Configurations:
  1. Set the HCLK to 400 MHz
  2. Enabled the CPU ICache and DCache (under Cortex_M7 Configuration)
  3. Enabled MPU (Region0, Region1 & Region2)
  4. Enabled LWIP
  5. Selected LAN8742 as the Driver_PHY (under LwIP>Platform Settings)
  6. DHCP disabled (IP, MASK: 255,255,255,000 , Gateway: Modem IP)
  7. RTOS disabled
  8. LWIP_HTTPD (LWIP_HTTPD_CGI & LWIP_HTTPD_SSI enabled)
  9. LWIP_HTTPD_MAX_TAG_NAME_LEN set to 16
  10. ICMP enabled (LWIP_BROADCAST_PING and LWIP_MULTICAST_PING in LwIP Key Options>IPMP Options).
  11. Code Generated for Keil V5
  12. MX_LWIP_Process added to the main function in While loop.
while(1)
{
MX_LWIP_Process();
}

I don't know how should I configure the CubeMX or change the generated code to be able to ping my board.

9 REPLIES 9
CodesMagic
Associate II

I'm trying for two months and still not able to ping my board.

... Any supports for STM32H743ZI Nucleo 144 board?

Hiren
Associate III

same face this problem in my stm32h743zi neculo board. if have any code for Ethernet UDP example please share us

kurta999
Senior

I was able to successfully awake LwIP on H747ZI and on F4 (on F4, CubeMX generated code worked), but not the one which is in CubeMX. A freshly generated project immendiately throws an ethernet DMA error on H7.

Finally I found an example in CubeMX package, located in: STM32Cube\Repository\STM32Cube_FW_H7_V1.4.0\Projects\NUCLEO-H743ZI\Applications\LwIP\LwIP_HTTP_Server_Netconn_RTOS and it works. Compiled with Atollic true studio (open SW4STM32\STM32H743ZI_Nucleo) and it will compile.

Try to use this example as starting point.

A very simple UDP echo example is here:

struct netbuf *buf;
static void udp_thread(void *arg)
{
	struct netconn *conn;
	err_t err;
	char buffer[256];
 
	/* Create a new TCP connection handle */
	conn = netconn_new(NETCONN_UDP);
	netconn_bind(conn, IP_ADDR_ANY, 1234);
	while (1)
	{
		err = netconn_recv(conn, &buf);
		if (err == ERR_OK)
		{
		  /*  no need netconn_connect here, since the netbuf contains the address */
		  netbuf_copy(buf, buffer, sizeof(buffer));
		  err = netconn_send(conn, buf);
		  netbuf_delete(buf);
		}
	}
}
 
sys_thread_new("UDP2TH", udp_thread, NULL, 2048, 4);

Hiren
Associate III

Thanks for reply.

i not use RTOS. i seen stl32h743Zi example but it code is rtos based and also no any found code on UDP based 

i also generated using Mx cube but it does not work.

1. i faces some warning "The ETH can work only when RAM is 

  pointing at 0x24000000"

  I was searching but did not find how to solve that.

2. I wrote code for ping command reply but it is not worked

GPIO pin mapping

PA1 ETH_REF_CLK

PA2 ETH_MDIO

PA7 ETH_CRS_DV

PB13 ETH_TXD1

PC1 ETH_MDC n/a

PC4 ETH_RXD0

PC5 ETH_RXD1

PG11 ETH_TX_EN

PG13 ETH_TXD0

Enable 

ICMP option

code

 while (1)

 {

  /* USER CODE END WHILE */

 MX_LWIP_Process();

  /* USER CODE BEGIN 3 */

 }

so i required UDP based example on STM32h743zi series.

if have you so please provide us 

Reguard's

Hiren

Thanks for reply.

i not use RTOS. i seen stl32h743Zi example but it code is rtos based and also no any found code on UDP based 

i also generated using Mx cube but it does not work.

1. i faces some warning "The ETH can work only when RAM is 

  pointing at 0x24000000"

  I was searching but did not find how to solve that.

2. I wrote code for ping command reply but it is not worked

GPIO pin mapping

PA1 ETH_REF_CLK

PA2 ETH_MDIO

PA7 ETH_CRS_DV

PB13 ETH_TXD1

PC1 ETH_MDC n/a

PC4 ETH_RXD0

PC5 ETH_RXD1

PG11 ETH_TX_EN

PG13 ETH_TXD0

Enable 

ICMP option

code

 while (1)

 {

  /* USER CODE END WHILE */

 MX_LWIP_Process();

  /* USER CODE BEGIN 3 */

 }

so i required UDP based example on STM32h743zi series.

if have you so please provide us 

Reguard's

Hiren

kurta999
Senior

Why you don't using RTOS? It much easyer to do with RTOS.

As I said above look after example which I linked, there complete lwip stack works. If one one CubeMX is broken then drop cube and use that example as starting point.

alister
Lead

Also see https://community.st.com/s/question/0D50X0000C6eNNSSQ2/bug-fixes-stm32h7-ethernet. If you use the code there, please post there it's working for you or any questions.

Piranha
Chief II

> It much easyer to do with RTOS.

Oh, really? That's why ST's brainless code monkeys still haven't understood multi-threading since the year 2007, right? 🙂 Actually, if one has a decent cooperative scheduler and software timers, then implementing lwIP for simple projects is easier without RTOS. But, if the project is complex or has real-time requirements, then it's "easier" to do it with RTOS.

Hi,

thanks for your comment,

can you please share your .ioc file (cube mx file )

Thanks