cancel
Showing results for 
Search instead for 
Did you mean: 

Can we save the text file in STM32F373C8 flash and it should detected when connected to computer via USB. Please let me know

TH U
Associate

Dear all,

I want to save my data in the form of text file in the flash memory of the controller STM32F373C8. And it can be retrieve when it is connected to the PC via USB, Is this controller is suitable for my application. If yes please give me the reason for which specification of the controller make this one to happen. If no please suggest me the suitable controller for this application. Because I am new to ST micro controller.

Thanks and Regards,

Thippeswamy H U

1 REPLY 1
SHing.137
Associate

Hello Sir,

I am also looking for same application.

I am using Nucleo-144 STM32L4R5 board.

I configured USB Data Plus and Minus pin and USB device class in Cubemx.

I am using Keil IDE.

Have you got the solution for your question?

or Could you please guide me for this.