cancel
Showing results for 
Search instead for 
Did you mean: 

usb bootloader

dieter 123
Associate III

Hi

(All?) my nucleo board(s) is/are detected as a USB device in windows. I can drag and drop a firmware binary on them. And the Firmware is automatically updated after power cycling the board.

I want to design my own board and use the USB to update the firmware via windows and USB.

Where will I find the source code for this feature?

Br

3 REPLIES 3

That's an mBed function within the ST-LINK's firmware

For STM32 USB update look at DFU examples, or use the built in boot-loader

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
dieter 123
Associate III

what is the "built in bootloader"? Do you have a link?