cancel
Showing results for 
Search instead for 
Did you mean: 

stm3f373 clock and flash latency setting

gazam
Associate
Posted on March 04, 2016 at 09:19

I worked with stm32f373.

To reduce power consumption I change the Hclk to 24Mhz and 48Mhz System clock.

(use AHB prescaler to /2)

But I confused by flash setting.

reference manual said that the latency is

000: Zero wait state, if 0 < SYSCLK? 24 MHz

001: One wait state, if 24 MHz < SYSCLK ? 48 MHz

010: Two wait sates, if 48 < SYSCLK ? 72 MHz

but the st library source code said that the latency is choosed by Hclk  not system clock

what is correct?

and what should I consider when the sys clk different with Hclk ?

#stm32
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Amel NASRI
ST Employee
Posted on March 04, 2016 at 15:21

Hi choi.gazam,

The number of wait states depends on HCLK range.

The description should be reviewed in the reference manual. 

Thanks for highlighting this.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Amel NASRI
ST Employee
Posted on March 04, 2016 at 15:21

Hi choi.gazam,

The number of wait states depends on HCLK range.

The description should be reviewed in the reference manual. 

Thanks for highlighting this.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.