cancel
Showing results for 
Search instead for 
Did you mean: 

break points are not accepted

raunaque
Associate II
Posted on October 27, 2004 at 05:59

break points are not accepted

5 REPLIES 5
raunaque
Associate II
Posted on October 27, 2004 at 04:08

Hi all

i am working on ST7 device. I am using indart kit. i am trying to put breakpoints in some lones of the code but while i am debugging it i am getting error '' one or more breakpoints are not positioned in valid files( no debug information or not a project file ). These breakpoints are then removed''

and the breakpoints are removed . can anybody tell what mistake i am doing

thanks in advance

Ronnie
marco32
Associate II
Posted on October 27, 2004 at 04:36

I had also that problem, but it's solved.

See Indart forum site:

http://www.softecmicro.com/forum/forumdisplay.php?s=8a31d48df485973a088a70dfa5435c55&forumid=3

Thread: Breakpoints

(Problem was the *.map file)
raunaque
Associate II
Posted on October 27, 2004 at 05:14

hi

the address u gave me says to apply break points before debugging and i am doing the same thing but then also i get the same message . So can u give some more solution to these issue

thanks

ronnie

marco32
Associate II
Posted on October 27, 2004 at 05:42

Can you show you'r build file?

raunaque
Associate II
Posted on October 27, 2004 at 05:59

i have one more problem friend

i am burning the firmware on the device but the device decriptor of the device is shown zero and all the descriptor is also 0x0 .i am able to see the descriptor by using the software . can u tell me what is the problem

i am also attaching the make file

thanks

PRODUCT = 7265

SIZE = 32K

ENV = default.env

CC = $(COMP) $(FLAGS)

CONF = mcu_conf.h map_$(PRODUCT).h

USBH = usb_reg.h usb_def.h usb_lib.h usb_eps.h user_usb.h

#************************** OBJECT FILES DEFINES ******************************

USB_LIST = usb_lib.o usb_int.o usb_ep1.o usb_ep2.o usb_eps.o

OBJ_LIST = main.o application.o map_$(PRODUCT).o descriptor.o user_usb.o jtag_state.o RDI.o

#******************************************************************************

USB_FS_$(PRODUCT)_$(SIZE).abs : $(ENV) $(OBJ_LIST) usb.lib USB_FS_$(PRODUCT)_$(SIZE).prm

$(LINK) USB_FS_$(PRODUCT)_$(SIZE).prm

#*** BURNING ***

$(BURN) -f Burner_$(PRODUCT)_$(SIZE).cmd

#******************************************************************************

main.o: $(ENV) main.c usb_lib.h $(CONF)

$(CC) main.c

RDI.o: $(ENV) RDI.c RDI.h

$(CC) RDI.c

jtag_state.o: $(ENV) jtag_state.c

$(CC) jtag_state.c

application.o: $(ENV) application.c $(CONF) $(USBH)

$(CC) application.c

map_$(PRODUCT).o : $(ENV) map_$(PRODUCT).c

$(CC) map_$(PRODUCT).c

user_usb.o : $(ENV) user_usb.c $(USBH) $(CONF) descriptor.h

$(CC) user_usb.c

descriptor.o : $(ENV) descriptor.c descriptor.h usb_lib.h

$(CC) descriptor.c

#***** USB files **************************************************************

usb.lib: $(ENV) $(USB_LIST) usb_lib_$(PRODUCT).ln

$(LIBM) usb_lib_$(PRODUCT).ln

usb_lib.o : $(ENV) usb_lib.c $(CONF) $(USBH)

$(CC) usb_lib.c

int_usb.o : $(ENV) int_usb.c $(CONF) $(USBH)

$(CC) int_usb.c

usb_int.o: $(ENV) usb_int.c mcu_conf.h usb_libs.h $(USBH)

$(CC) usb_int.c

usb_ep1.o : $(ENV) $(CONF) $(USBH) usb_ep1.c

$(CC) usb_ep1.c

usb_ep2.o : $(ENV) $(CONF) $(USBH) usb_ep2.c

$(CC) usb_ep2.c

usb_eps.o: usb_eps.h usb_eps.c

$(CC) usb_eps.c

# EOF