cancel
Showing results for 
Search instead for 
Did you mean: 

Power Supply

Bruno Brentegani
Associate II
Posted on January 18, 2018 at 11:14

Hi all, i'm using STM32F407VG Discovery with expansion board. I have two questions:

1 - Why when i try to connect my smt32f4 using the 5V pin and the GND pin with an external power supply without a USB connection my C application sotred in the flash of my STM32 don't start (i try to remove the  ST-LINK jumpers on the board but the problem remains) 

2- Anyone know the maximum power consumption of the STM32F4 + EXP board... I see on my supply 160mA. It's too much?

Thank you very much for the answers!

Bruno

2 REPLIES 2
Posted on January 18, 2018 at 17:20

Check the version of the ST-LINK firmware in use. Seem to recall V25 being an issue with USB Charger type connections.

The jumpers just address the SWDIO/SWCLK pins, the ST-LINK still has a connection to NRST, and can clamp it low.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on January 18, 2018 at 17:50

Basic tests with volmeter to be sure that you powered the target MCU? Don't assume - just measure to be sure..