User Activity

I am trying to prototype ethernet on the NUCLEO-H7S3L8 eval board. When enabling ethernet through CubeMx using the same configuration I've used on the NUCLEO-H563ZI, the ethernet driver fails initialization. Is there an alternative Ethernet driver th...
I have a NUCLEO-H7S3L8 board, and I am unable to debug any of the projects. I receive a sigtrap error upon debugging. I have tried multiple projects in ST's Github. STM32CubeH7RS/Projects/NUCLEO-H7S3L8 at main · STMicroelectronics/STM32CubeH7RSAll pr...
1. Does the STM32MP157D-DK1 board have 3.0 USB ports? Does the USB C connector have USB 3.0 capabilities?2. If no to the questions above, what STM32MP board should we use if we want to have USB 3.0 capabilities?
I have created a very minimal prototype project with ThreadX on the NUCLEO-H563ZI board. I have a single task that blinks a LED on and off. I would like to prove out an example with FileX using SRAM. I have enabled FileX via CubeMX with the default s...
Hello, I'm trying to find more information regarding ThreadX's on-the-fly properties update feature. In the ST Wiki article, there is mention of this feature, but none of the links and webpages seem to provide any details regarding what this feature ...
Kudos from
Kudos given to