Hi, the STSPIN240 datasheet states that the absolute maximum ratings for logic input voltage should be between -0.3V and 5.5V. However, it is unclear whether the logic input voltage can exceed VS.Can the logic input voltage exceed VS?Thanks,
Hi Peter, thank you for your response.Yes, I understand and agree with your comment.However, considering that the STSPIN240 has a supply voltage pin "VS" which can be powered with a voltage ranging from -0.3V to 11V, it is unclear whether the maximum...
Hi Andrew, thank you for your response.I reviewed the pinout as you suggested, and the F411RE is identical to the F401RE, which is compatible according to the STM32 Nucleo expansion boards Motor Control Selection Guide document. However, I'm wonderin...