User Activity

Hi All,I want to ask a general question regarding EEPROM with SPI Interface,I am not sure if I understand the Datasheet correctly however it mentions that I can clock in 64 bytes (with the CS line pulled Low) then it mention the EEPROM has a write ti...
Dear All,I am working for the first time with a production set of code and I am asking some help in the following question/ uncertainty ,The STM32F103Cx device has a phew Core exception IRQ's as shown below/****** Cortex-M3 Processor Exceptions Numb...
Hi All,I need some help ,I am pulling my hair out ,I declare a buffer of 40 Bytes  uint8_t myBuffer[40]= {0}; I then read a nunber of bytes from an EEPROM over SPI ,I have a logic analyser connected and can see the for example if I read 10 buytes at ...
Hi All,Please I need some explenations regarding EEPROM (with SPI interface) .The SPI is working I can see the signals on my LA ,However I have some very basic questions regarding the EEPROM 256Kx8 page size according to the datasheet is 64 bytes per...
Hi All,I need some help advise Please,I have an application in which I need to read 4 external ADC chips over SPI this is all working fine(spi and ADC conversions)The Application sample the ADC chips every 100uSec I have 4 buffers circular buffers on...