User Activity

I have recently picked up an old project which was build by a developer who has left the company.  For various security and compliance reasons, I need to know which specific libraries are linked to the project.  I can see from the project properties ...
This fault has appeared very abruptly.  One hour ago I was working with the board just fine, programming via STM32CubeIDE. Then I swapped the board to a different USB port on my laptop, now it is not programmable.When I hit the 'Run' button, it appea...
Hi all,I've been tasked with making some changes to an existing STM32 project. Unfortunately my predecessor was not keen on documentation, so I don't have much guidance on how the project was built in the past.I have pulled the project from our SVN s...
Hi all,I am having a very strange problem with an SPI read operation on the STM32F103ZG.I am using the SPI bus to read from an external ADC device. I am performing around 1000 reads per second and almost all of them are coming back perfectly, but onc...
Hi,I am having a problem where I am unable to run my code in debug mode from within STM32CubeIDE v1.15.I can program the device fine with STM32CubeProgrammer, but when I try to debug I get this output:log output file: C:\Users\[me]\AppData\Local\Temp...
Kudos from
Kudos given to