Error in final launch sequence - No device on target
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-05 3:43 AM
I have a NUCLEO-G491RE board connected to a PC running STM32CubeIDE v1.17.0. On first connection I was prompted to update the firmware on the board, which I did. On successful completion of the update I disconnected and reconnected the board, but the download failed with the attached message.
I have tried several USB cables and also with and without an intermediate USB hub to eliminate these possibilities.
What is the solution please?
Solved! Go to Solution.
- Labels:
-
STM32CubeIDE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-07 7:47 AM
Hello @alw ,
Further to the picture provided on message. I recommend that you change the jumper on CN11 to JP6.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-07 6:12 PM
Problem solved, it was just jumper link settings.
JP5 (5V_SEL): 5V_STLK
JP6 (IDD): On
JP7 (BOOT0): Off
Suggestion, rather than the error messages that are provided, have ones that advise users to check thatthese links are correctly fitted.

- « Previous
-
- 1
- 2
- Next »