User Activity

im using th nucleo-f446re board, and the st-link isn't there. Am i missing some jumper connection?  
Hi! I have a code that is supposed to develop CAN-bus communication, but these two functions go straight to error handler. Any suggestions why that might be? for reference I'm using the nucle-l433rc-p board.  
Hi I'm new in working with CAN-bus. My project involves two stm32 boards (both are nucleo-l433rc-p) and I want to get CAN-bus communication between them. The code is supposed to make a build in LED blink each time the blue button on the main nucleo b...
Hi I'm very new in working with CAN-bus. My project involves two stm32 boards (both are nucleo-l433rc-p) and I want to get CAN-bus communication between them. The code is supposed to make a build in LED blink each time the blue button on the main nuc...
Hi! I've seen some tutorials on can communication and notice that each of them use different StdId's. I'm using two nucle-l433rc-p boards, do I need a specific StdId or will any number between  0 and 0x7FF suffice?  
Kudos given to