cancel
Showing results for 
Search instead for 
Did you mean: 

How do I set correct stdID for CAN-BUS?

Mr4
Associate III

Hi! I've seen some tutorials on can communication and notice that each of them use different StdId's. I'm using two nucle-l433rc-p boards, do I need a specific StdId or will any number between  0 and 0x7FF suffice?

 

1 ACCEPTED SOLUTION

Accepted Solutions
mÆŽALLEm
ST Employee

Hello,

Standard ID is a 11bit field so the range is 0x0 - 0x7FF

For the Extended ID the field is 29-bit length. The range: 0x0 - 0x1FFF FFFF

Note that the ID is not the address of the node like I2C but any node could have many ID's. Each ID is specific to a function in the node.

The important thing: you need a unique ID on a bus for each function.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mÆŽALLEm
ST Employee

Hello,

Standard ID is a 11bit field so the range is 0x0 - 0x7FF

For the Extended ID the field is 29-bit length. The range: 0x0 - 0x1FFF FFFF

Note that the ID is not the address of the node like I2C but any node could have many ID's. Each ID is specific to a function in the node.

The important thing: you need a unique ID on a bus for each function.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.