Hello @liamur ,Have you considered changing the clock source, such as using PLL2R? Additionally, have you explored our BootCM4_CM7 template in the reference firmware package? This project offers a comprehensive reference template that can be utilized...
Hello @RiverDi_user ,Given that the SD card slot is integrated into the display module and you are using the SDMMC1 interface, could you please try to verify that the clock configuration for the SDMMC1 peripheral is correct? This could be a potential...
Hello @iyed_hamdi ,Thank you for bringing this matter to our attention, this issue has already been identified and reported in this thread:sdmmc not working with 4-bit mode but working only with 1-bit mode Best Regards,
Hello @iyed_hamdi ,Could you please provide a more detailed description of the issue you are encountering? Specifically, in which function does the code execution halt, and what is the return value of the instruction at that point? This information w...
Hello @Player_Saturn ,Your settings should be okay, could you pls check whether the EXTI13_IRQHandler function in your stm32h5xx_it.c file is executed when you press the button?If it is not, could you please specify the board you are working with so ...