User Activity

Hi,I have an STM32L412RBT6P microcontroller and a CFAG12864T3-NFH LCD which uses an ST7565 controller. I want to use SPI to communicate with the LCD and leverage DMA to efficiently transfer data with lowest current consumption possible. Could someone...
Hello everyone,I'm working on a circuit for monitoring the bias voltage of a GM tube, which requires a high voltage of 100V. I am currently using a OA1NP22C op-amp configured as a unity-gain buffer to read the divided voltage. To minimize current con...
Hello, I'm working on a project using the STM32L412RBT6P microcontroller, and I have a few questions regarding the use of the VDD12 pins to achieve the lowest possible power consumption. 1. Can I directly connect the two VDD12 pins to a 1.25V supply?...
Hello ST Community,I am currently working on a project that involves the use of 2 LIR2450 Li-ion batteries. For the battery charging aspect, I am seeking recommendations for a suitable Power Management Integrated Circuit (PMIC) charger from ST.Specif...