User Activity

Hello. I have a STM32H747XI project. This MCU has both CM4 and CM7 cores. I can reset both of them, when I use NVIC_SystemReset() function. How can I reset only CM7 core from CM4 core?
Hello,I've created a test touchGFX project for stm32h747i-disco by using TouchGFX Designer-4.21.4. It has only one screen that has one background image and one text. You can see it below:When I generate the code by using TouchGFX Designer-4.21.4 and ...
Hello,I have a STM32H747I-DISCO touchGFX project that has a 8-bit color depth and it is working very well, when I use external RAM for frame buffer. But when I disable external RAM and use internal RAM for the frame buffer by applying these instructi...
Hello,I have a stm32h747i-disco board. When I create a touchGFX project by using touchGFX designer template, it works perfectly. Its color depth is 24-bit and when I change color depth to 16-bit(RGB565), it fails.To change color depth to 16-bit, firs...