[Problem solved] The image can be downloaded to the target board and booted successfully via STM32CubeProgrammer [2023-12-15 Friday]I got a hint from the webpage "Populate the target and boot the image." Hint:STM32CubeProgrammer v2.14.0 is recommende...
I've used STM32CubeProgrammer to create partitions into micro SD cards in the STM32MP157F-DK2 development board. An error occurred and the STM32CubeProgrammer stopped working (as shown in the figure, log file attached).
1.I've tried different proxy settings (both "No Proxy" and "Use System Proxy Parameters").I clicked on check connection, and I got the green check instead of the red cross (as shown in the figure). 2.However, when I click on software update, the con...
I also encountered this problem today. The problem is still unsolved.In the beginning, I used STM32 Cube Programmer 2.12.0, and tried different proxy settings (both "No Proxy" and "Use System Proxy Parameters"). It didn't work. The server connection ...
I also encountered this problem today.In the beginning, I used STM32 Cube Programmer 2.12.0, and tried different proxy settings (both "No Proxy" and "Use System Proxy Parameters"). It didn't work. The server connection was still not established.Later...