2023-10-16 9:30 AM
Hi,
when starting STM32 Cube Programmer (W64) or checking for updates I get this message
There is "No Proxy" set in the Proxy settings and the Windows PC has internet access (browsing www works).
Any ideas?
Thanks,
M
Solved! Go to Solution.
2023-11-17 10:03 PM
1.
I've tried different proxy settings (both "No Proxy" and "Use System Proxy Parameters").
I clicked on check connection, and I got the green check instead of the red cross (as shown in the figure).
2.
However, when I click on software update, the connection error occurs (as shown in the figure).
------------------------
System Information:
Use VMware
DISTRIB_DESCRIPTION="Ubuntu 22.04.3 LTS" provided by osboxes.org
STM32CubeProgrammer, version 2.14.0
I've checked my network connection. The web browser can normally connected to the internet.
2023-11-21 7:13 AM
2023-12-17 7:18 PM - edited 2023-12-17 7:20 PM
[Problem solved] The image can be downloaded to the target board and booted successfully via STM32CubeProgrammer
[2023-12-15 Friday]
I got a hint from the webpage "Populate the target and boot the image."
Hint:
STM32CubeProgrammer v2.14.0 is recommended for ecosystem release v5.0.0
REF: https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Let%27s_start/Populate_the_target_and_boot_the_image
Hence, I tried to use Ecosystem v5.0.0 and chose the "FlashLayout_sdcard_stm32mp157F-dk2-optee.tsv" file in the Starter Package.
It works. The image was downloaded to the target board and booted successfully.
[2023-12-18 Monday]
I tried to use Ecosystem v5.0.0 and chose the "FlashLayout_sdcard_stm32mp157f-dk2-extensible.tsv" file in the Starter Package.
It works. The image was downloaded to the target board and booted successfully.
NOTE: [Filename inconsistancy]
The tar.gz filenames of the starter package stated in the webpages "Populate the target and boot the image" and "STM32MP1-Ecosystem-v5.0.0 Starter Package" are not the same.
It is "en.flash-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz" in the webpage "Populate the target and boot the image"
REF: https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Let%27s_start/Populate_the_target_and_boot_the_image
It is "en.flash-stm32mp1-openstlinux-6-1-yocto-mickledore-mp1-v23-06-21.tar.gz" in the webpage "STM32MP1-Ecosystem-v5.0.0 Starter Package"
REF: https://www.st.com/en/embedded-software/stm32mp1starter.html#get-software
Hence, the command "tar xvf en.flash-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz" shown in the webpage "Populate the target and boot the image" cannot be copied, pasted, and used directly.
-----------------------------
[System information]
Operation system: VMware, DISTRIB_DESCRIPTION="Ubuntu 22.04.3 LTS" provided by osboxes.org
Target board: STM32MP157F-DK2
STM32CubeProgrammer version: 2.14
Ecosystem version: 5.0.0