User Activity

I am running a bluetooth application using freeRTOS on a Nucleo-WB55 (STM32WB55RG). I am in the process of implementing Emulated EEPROM (X-Cube-EEPROM) to store som data. After implementing eeprom emulated in a ble_heartrate_freertos example I have h...
I have a custom board, which is based on the STEVAL-SPIN3201, it is used to control a low inductance BLDC motor with hall-sensors (100µH). The motor controller is running and is able to control the motor. Unfortunately the phase currents tell that th...
I have a custom board with a STMWB55 (master) and a STM32F031 (slave). They communicate over SPI using DMA. Unforturenately there are communication problems.   In order to identify the problem I have simplified the setup. I have used a ST NUCLEO-F031...
Hello ST Community, I have setup a SPI master and a SPI slave, both use DMA in Normal mode. The word size is 8-bits and the data size is 8-bytes. The problem is that the slave transmits messages which contains old data. When it should send:MISO: { 0x...
Hello, I am working on a motor control project that is to be driven battery-powered. This means that the DC current has to be monitored in order to avoid overloading the battery. I have made a Control Loop which takes in a DC Current reference as inp...
Kudos from
Kudos given to