User Activity

Hello,I am using a STM32F427 to read and write data to EEPROM Serial 256-Kb SPICAT25256. I use LL API, and DMA full-duplex over SPI. I manage myself the Chip Slect signal.I can see with logic analyser that datas are sent and received to/from EEPROM c...
Hello,I'm using BLE_p2pClient and BLE_p2pServer programs.I had pairing request in BLE_p2pClient to have both devices bonded.Now, I want to have a fast connection between client and server; actually, the connection between client and server is about 2...
Hello,I'm trying to flash \STM32Cube_FW_WB_V1.18.0\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB1x\stm32wb1x_BLE_Stack_full_fw.bin at address 0x08021000 with SMTCubProgrammer version 2.14.0I think that it is unsuccessful, and the application BL2_p...
Hello,What I have done:- Following instructions from AN5185 document.- Using STM32CubeProgrammer v2.14.0- NUCLEO-WB15CC powered on- With STM32CubeProgrammer :- ST-Link configurationST-Link upgrade (v3.12.3)Update to firmware V2J42M27- ST-Link Connect...
 Hello,I am downloading the firmware \STM32Cube_FW_WB_V1.17.0\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB1x\stm32wb1x_BLE_Stack_full_fw.bin to the STM32WB15CC using STM32CubeProgrammer v2.14.0, with USB cable.At the end, I have :    11:21:53:481...