cancel
Showing results for 
Search instead for 
Did you mean: 

"Error: failed to download Segment[0]" while downloading firmware to STM32WB15CC with STM32CubeProgr

FWX
Associate III

 Hello,

I am downloading the firmware \STM32Cube_FW_WB_V1.17.0\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB1x\stm32wb1x_BLE_Stack_full_fw.bin to the STM32WB15CC using STM32CubeProgrammer v2.14.0, with USB cable.


At the end, I have :

    11:21:53:481 : Error: failed to download Segment[0]
    11:21:53:481 : Error: failed to download the File

 

If I try to download  stm32wb1x_Safeboot_fw.bin,  there is no error.

Where is the problem ? All products are from STMicroelectronics...

Thank you for help.

                                               FWX.

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi Remy,

Thank you for the link and your useful explanations.
Best regards,

                                    FWX.

View solution in original post

2 REPLIES 2
Remy ISSALYS
ST Employee

Hello,

In this wiki page, all steps to update the wireless stack are described, can you check if your sequence it's the same or not? In addition, according to the release note the install address for BLE Full Stack v1.17.0 on WB15 is 0x08021000.

Best Regards

Hi Remy,

Thank you for the link and your useful explanations.
Best regards,

                                    FWX.