cancel
Showing results for 
Search instead for 
Did you mean: 

ST_Link support in SEGGER EMBEDDED STUDIO

Aks
Associate III

Hello

 

We have a few queries regarding the use of ST-Link for debugging, and I would greatly appreciate your assistance in this matter.

  1. We are currently using a J-Link Base probe for debugging the STM32MP157F processor in SEGGER EMBEDDED STUDIO, and we are successfully performing multi-core debugging with the J-Link.Could you please confirm if ST-Link can be used to debug the A7 core in SEGGER Embedded Studio? If so, could you kindly provide the necessary settings or configuration required for debugging using ST-Link, as well as the process for performing multi-core debugging with ST-Link?
  1. We are also planning to work with the STM32MP257 processor in the near future. Could you please recommend an ST-Link model that is compatible with both the STM32MP157F and STM32MP257F processors?

 

Thanks & Regards

Akshitha Pattem

5 REPLIES 5
Andrew Neil
Super User

As the name suggests, Segger Embedded Studio is a Segger product - not ST - so you need to go to Segger for support with their tool!

https://www.segger.com/products/development-tools/embedded-studio/

https://www.segger.com/support/technical-support/

https://forum.segger.com/index.php/Board/9-SEGGER-Embedded-Studio-related/?s=a46e1686f66f049595ceb67cf796f7bf771bb244

 

AIUI, Segger Embedded Studio is for microcontroller development - not MPUs ?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Olivier GALLIEN
ST Employee

Hi @Aks 

 

I confirm there's no plan in ST to support STM32MPU product in SEGGER EMBEDDED STUDIO. 

We recommand to use STM32CubeIDE fully supported. 

 

ST-LINK V3 probe is compatible with both  STM32MP157F and STM32MP257F 

 

Olivier 

 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @Olivier GALLIEN 

I apologise for the late reply.We greatly appreciate your suggestion and keep that in mind while moving forward.

 

Thanks & Regards

Akshitha Pattem 

 

 

Hello  @Andrew Neil 

I apologise for the late reply.

Thank you for  response. Segger Embedded Studio supports development of MPUs too.

Thanks & Regards

Akshitha Pattem

 

If your question has now been answered, please mark the solution:

https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.