User Activity

Hello STM Comunity, I am making this post because I have reviewed many reference schematics for the use of the STM32F103C8T6, and in most of them, I see that they use 20pF load capacitors for the LSE circuit.The datasheet literally states that the va...
Hello all,I'm working on a project with the STM32F103C8T6 microcontroller, using STMCubeIDE STM32CubeIDE Version: 1.13.2, and the HAL STM32Cube FW 1.8.5. In the example program I've attached, I set an alarm for 00:00:00, and once the alarm interrupt ...
Hello,In this thread, I would like to clarify a point regarding how to read the RTC_CLR[ALRF] flag. I am using the STM32F103C8T6 microcontroller and the STM32Cube Firmware (HAL) version 1.8.5. This flag indicates that the alarm has been activated.My ...
Kudos from
Kudos given to