User Activity

Completed the STM CAN 2 Node tutorial and created the set up successfully. Have Spark Max and NEO motors in robot with RoboRio . However would like to do a breadboard set up less another Rio ( expensive ) . Just to function a 2 Node CAN ( micro & mot...
A Beginner's inquiry please be patient Local host error in the debugger configuration, ID of both boards ( STMH743ZI2 ) and the updated firmware verified in the " help" update .. Could it be that the " canned " local host " from the download files is...
Yes it is a common problem - just can't find  the problem  -  Download  FDCAN  Files from Youtube controllers site.Software side -IDE,MX  files  okay  except when I get to debug configuration - Error" nost link "   drivers exist in Device Manager  ; ...
AS  in the  TUTORIAL  FDCAN NORMAL OPERATING MODE , What pin on the NUCLEO H743ZI2 -144 board  receives the VVD  ( and  VIO ) from the Transceiver MCP2526FD 8DIP  see attached  Is it a plug in or do I need to create a contact pt . 
Not sure this is the right label Is there  a link  where I can obtain the complete program code for STM32 FDCAN in NORMAL MODE for the STM32H745I-DISCO ( Tutorial ) similar to the entire code MULTI Can .zip  that was found i the link for the STM32 Ca...
Kudos from
Kudos given to