cancel
Showing results for 
Search instead for 
Did you mean: 

FD CAN TRANSCEIVER MCP2562FD VVD Hook UP to NUCLEO H743ZI2

MROWL
Associate III

AS  in the  TUTORIAL  FDCAN NORMAL OPERATING MODE , What pin on the NUCLEO H743ZI2 -144 board  receives the VVD  ( and  VIO ) from the Transceiver MCP2526FD 8DIP  see attached  Is it a plug in or do I need to create a contact pt . 

20231201_165525[1].jpgScreenshot 2023-12-01 165727.png

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

VDD and VIO are power pins and should be connected to a power rail appropriate for the chip according to the datasheet. VDD needs 5V and VIO can take 5V or 3.3V. You should be able to find pins on the nucleo board which supply these voltages.

TDK_0-1701610924829.png

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
TDK
Guru

VDD and VIO are power pins and should be connected to a power rail appropriate for the chip according to the datasheet. VDD needs 5V and VIO can take 5V or 3.3V. You should be able to find pins on the nucleo board which supply these voltages.

TDK_0-1701610924829.png

 

If you feel a post has answered your question, please click "Accept as Solution".
MROWL
Associate III

Thanks

sana1
Associate III

you communicate can FD with this solution !