2020-11-19 11:32 AM
When I try to install the workshop materials I get this file removed from Avast Antvirus stating that it is not save to install. Is this expected or something weird is going on my machine?
2020-11-19 05:24 PM
Dear STMicroelectronics,
Hereby, I would like to confirm that my system also blocked the application due to security reason.
'Windows SmartScreen Filter disabled unrecognized application. Running this application can harm the system.
Origin: Unknown
Application: STM32H72x3xWS-material_1.0.exe'
No other message is provided, so further diagnostic is not feasible at the moment.
Best regards,
Krzysztof Szynalski
Sr. Design Engineer
MD DE DUVA D WAFER HANDLING & POS
Location 07.D.05 (ABW)
ASML Netherlands
2020-11-20 01:19 AM
Dear @K_Szynalski and @ADonc.1 ,
thank you for pointing to this issue. I uploaded to the google drive a ZIP file with the content of the installer, so you should be able to install the necessary tools and materials manually. You should be able to access the file via same link.
I also updated the PDF with the steps required for manual installation.
Sorry for the inconvenience.
Best regards,
Adam Berlinger
2020-11-20 01:35 AM
@Adam BERLINGER Thank you Adam!